A Emerson amplia suas capacidades de serviço para atender às necessidades mais importantes dos clientes

Smart project and support service connections bridge critical gaps in customer resources

ANAHEIM, CALIF (October 8, 2012) -- Emerson Process Management has added more than 4000 service personnel since 2005 and plans to increase its global service staff at approximately twice the industry growth rate for the next four years. The rapid growth is part of a strategic expansion of project and support services to meet customers’ growing needs. 

Today’s economics require that most process manufacturers have only the staff necessary to maintain efficient operations. This leads to a “capabilities gap” when substantial new capital investments are undertaken or when maintenance requirements spike, as during plant turnaround.  Emerson’s expanded service capabilities help customers meet the challenges of both situations. 

“The number of large automation projects for which we’ve been chosen – increasingly as Main Automation Contractor -- has dramatically increased in the past two years,” explained Steve Sonnenberg, president of Emerson Process Management.  “Many of these projects are in emerging markets, often focused on meeting critical infrastructure needs or developing natural resources.  Not only do they require large amounts of engineering effort for design, commissioning, and startup, but once they’re up and running they need prompt, dependable support services to stay at peak efficiency.”

Process manufacturers also realize that achieving best-in-class operations often requires adopting new technology, but they are not necessarily staffed to implement major technology initiatives. Emerson can also help them bridge this gap by providing contract personnel to do initial setup of new technology approaches and assist with ongoing support programs. 

“We are very pleased that our customers are opting to meet their project and service needs by partnering with Emerson Process Management,” said Sonnenberg.  “It’s our goal to address the gaps in our customers’ in-house capabilities with our quality services. The aggressive investment program we’ve put in place will help us meet those needs.”

Mídia:
• Contatos: Contatos de mídia global da Emerson

Outros recursos:
• Participe da comunidade Emerson Exchange 365
• Siga a Emerson no X Facebook LinkedIn YouTube

Sobre a Emerson 
Emerson (NYSE: EMR) é uma empresa global de tecnologia e software que fornece soluções inovadoras para os clientes dos mercados industrial, comercial e de consumo. Por meio de seu portfólio de automação, que é líder de mercado, além de sua participação majoritária na AspenTech, a Emerson ajuda fabricantes híbridos, de processo e discretos na otimização de suas operações, na proteção de seus funcionários, na redução de emissões e na realização de metas de sustentabilidade. Para mais informações, acesse Emerson.com.


Ative o JavaScript para usar este site.