Superior Wetgas Metering Performance

Superior Wetgas Metering Performance without Compromise

As the industry evolves and faces new challenges, Emerson is continuously developing and improving its measurement
solutions. As an answer to the current and future industry requirements, Emerson now offers the latest generation Roxar Subsea
Wetgas Meter, providing an optimal solution with no technology compromises.The Roxar Subsea Wetgas Meter has an unparalleled 15-years track record in some of the world’s most challenging wet gas fields all over the world.

자세히 보기...
클릭하여 계속 읽기 Superior Wetgas Metering Performance without Compromise

Application

The challenges and risks with formation water breakthrough

The Roxar Subsea Wetgas Meter (SWGM) addresses the following operator challenges related to formation water breakthrough:

  • Increases risks of hydrate formation and therefore the need for increased Mono-ethylene glycol (MEG) injection
  • Jeopardizes hydrocarbon production due to water coning in the reservoir
  • Increases water flow and injected chemicals in lieu of hydrocarbon production
  • Pipeline scaling
  • Pipeline corrosion and erosion

The critical time window of a hydrate plug forming

There are field examples where the period from formation of water breakthrough, to hydrate growth and build-up and pipeline plugging is less than 20 minutes. Therefore, rapid, highly sensitive measurements are needed to capture the critical time window of a hydrate plug forming in order to take remedial actions to save the well. The Roxar Subsea Wetgas Meter has the ability to instantaneously measure extremely small changes in water volume fraction, as little as ± 0.00002 % (0.2 ppm).

Ensure reliability of hydrocarbon supply

The lack of real-time accurate hydrocarbon
measurements impacts allocation strategies and obligations. There is a need for a meter that provides accurate and robust measurements across multiple reservoir conditions. Only Emerson has dedicated subsea wetgas meters that address application specific challenges

Measurements on a well-by-well basis for production optimization

Case study offshore Egypt: Installation of  Roxar Subsea Wetgas Meters has helped the operator to monitor water production profiles in real-time. By providing early warnings of the water produced, meters installed on the field have helped the operator and its partners save several wells from water breakthrough. It has also provided the operator with the necessary information to optimize the performance of its wells, leading to increased availability.

이 웹 사이트를 사용하려면 JavaScript를 활성화하세요.