Mining Application

Hydrocyclone Feed and Discharge Isolation

Extend hydrocyclone maintenance intervals using time-tested knife gate valves for feed and discharge isolation of abrasive slurry media.
hero-h003-classification

Better Performing Hydrocyclones With Reliable Feed Isolation

Hydrocyclones separate and classify fine and coarse materials prior to flotation. Fines, or right sized particles, pass through the top of the hydrocyclone (vortex) for processing, while heavier solids discharge though the bottom of the hydrocyclone (apex) and back to regrind or directly to tailings. Isolating the hydrocyclone feed allows the system to maintain pressure, volume and separation.

Przeczytaj więcej
Kliknij, aby kontynuować czytanie Better Performing Hydrocyclones With Reliable Feed Isolation

Expert Insights

Isolation Knife Gate Valve for Medium-Slurry Mining and Minerals...

Many manufacturing processes have challenging fluids flowing through their pipes and vessels. Mining and minerals have some of the most challenging with abrasive and corrosive solids in the flowing fluids. In a Valve magazine article, Challenges of Medium Density Slurry Service in Mining and Mineral Processing, Emerson’s Mike Gordon describes innovations in knife gate valve …

przeczytaj więcej
Improved Mining Operations by Detecting Roping and Plugging on...

Author: Douglas Morris One of the most ubiquitous operations in any mine is the use of hydrocyclones (cyclones) in the comminution circuit to sort particle sizes for mineral processing. Downstream of this process is the flotation circuit, which can be adversely affected if there is an upset with cyclones. Poor cyclone performance will impact recovery, …

przeczytaj więcej
Success in a Challenging Tailings Relocation Project

An Australian coal mining company was looking to extend the life of its mine. The challenge was that the area where they wanted to expand mining operations was currently being used as a tailings storage facility (TSF).

przeczytaj więcej
Włącz skrypt JavaScript aby skorzystać z tej strony internetowej.