Emerson’s Latest Control System Transforms Projects and Helps Bridge IT/OT Divide for Operational Performance

1802-DeltaV-control-system-version-14 (2)

The new DeltaV Live Operator Interface, part of DeltaV version 14, brings an entirely new and intuitive user experience, making it easier for operators to quickly understand and safely respond to changing plant conditions. High Resolution Image


1802-DeltaV-control-system-version-14 (3)

The DeltaV Live Operator Interface enables the intuitive user experience plant operators experience in the control room to follow them on tablets and phones. High Resolution Image


1802-DeltaV-control-system-version-14 (5)

Emerson’s latest release of the DeltaV automation system brings significant enhancements across software, hardware, and mobile apps to establish a cybersecurity-certified control system with a modern user experience that keeps plant operators more connected, informed, and efficient.  High Resolution Image


1802-DeltaV-control-system-version-14 (6)

Emerson’s Smart Commissioning software, upgraded as part of DeltaV version 14, brings the time it takes to commission devices down from 25 minutes to as little as 10 minutes. High Resolution Image


1802-DeltaV-control-system-version-14 (4)

The DeltaV PK Controller enables plants to control skids and applications typically managed by PLCs with a standalone DeltaV controller or connect into an integrated full-scale DCS automation architecture. High Resolution Image


1802-DeltaV-control-system-version-14 (1)

Emerson’s DeltaV Mobile platform natively connects into DeltaV—securely and without additional engineering—to enable managers, engineers, operators and subject matter experts to monitor operations and have critical data and alarms at their fingertips, whenever and wherever they need it.. High Resolution Image

New release of DeltaV™ control system makes project engineering and operations more intuitive, flexible, accessible and secure

AUSTIN, TEXAS (February 12, 2018) – Emerson is expanding its Plantweb™ digital ecosystem with today’s launch of DeltaV version 14, a cybersecurity-certified control system designed to deliver new value in capital projects and make plant operations more connected and productive. The latest release provides significant innovations to the entire DeltaV architecture and was built with customers’ digital transformation initiatives in mind.

This major update to the DeltaV automation system includes several meaningful enhancements to eliminate costs and reduce complexity in capital projects, plus improve productivity during operations through enhanced access to production and equipment data, improved usability and greater security.

“More than ever, an integrated plant data environment is essential to achieve digital transformation. With DeltaV, we’re reducing the engineering effort required to securely connect plant, operational and information systems,” said Jamie Froedge, president of Process Systems and Solutions, Emerson Automation Solutions. “Our customers will have more capabilities in their distributed control and safety systems to help them successfully execute capital projects and optimize operations.”

Capital Project Flexibility
Continuing to advance the impact of DeltaV Electronic Marshalling with CHARMs on capital project engineering, CHARM I/O Block takes CHARMs—which achieved more than one million deployments at more than 1100 sites in only five years—closer to the field. Small enclosures with up to 12 CHARMs can now be installed closer to field devices, significantly reducing wiring and overall installation costs by as much as 60 percent and providing more engineering flexibility.

Smart Commissioning, launched in 2016, took one of most engineering intensive operations off a project’s critical path. Traditionally, commissioning has been a manual task that requires more than two hours per device for thousands of devices. Smart Commissioning reduced commissioning time to 25 minutes. Emerson is now expanding these capabilities and reducing device commissioning time to as little as 10 minutes, a nearly 93 percent reduction in costly commissioning time that could save several hundred-thousand dollars in engineering costs.

Mobility and User Experience
DeltaV Live Operator Interface is a modem, built-for-purpose operations experience that is easy to understand and modify. The HMI comes pre-engineered with the industry's best practices for user experience including ISA 101.01 and is based on research with the Center for Operator Performance, a consortium of vendors and academia focused on human factors engineering. The HTML5 interface enables scalable graphics and gives operators the flexibility to adjust their displays to focus on process data that is most important for each situation. The new operator interface helps improve overall situational awareness and decision-making speed. Emerson is helping companies prepare for the shift to mobility with DeltaV Live by building a foundation for graphics to be transferrable across desktops, laptops, and mobile devices—all without additional engineering or custom scripting.

A Secure, Connected Plant
DeltaV will offer its users a new level of confidence and protection from cybersecurity threats by being one of the only systems to have a top-to-bottom cybersecurity certification. DeltaV v14 will be certified ISASecure SSA Level 1 by the International Society of Automation (ISA), signifying that Emerson developers are trained to write secure code and the system as a whole is hardened against cyber threats.

Emerson is making connecting a plant’s OT systems with IT systems seamless by expanding OPC UA access in its DeltaV hardware and software offerings. DeltaV is the pathway for most plant data and now using the IIoT’s most prevalent protocol, OPC UA, DeltaV applications and servers can securely share data to cloud analytics applications, remote monitoring solutions, and third-party technologies.

Emerson announced the first two additions of its new DeltaV system last year with the DeltaV PK Controller and DeltaV Mobile. The DeltaV PK Controller enables plants to control skids and applications typically managed by PLCs with a standalone DeltaV controller or connect into an integrated full-scale DCS automation architecture or the cloud via embedded OPC UA. The DeltaV Mobile platform that natively connects into DeltaV—securely and without additional engineering—to enable managers, engineers, operators and subject matter experts to monitor operations and have critical data and alarms at their fingertips, whenever and wherever they need it.

For more information on DeltaV, visit Emerson.com/DeltaV14.

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson on Wechat

About Emerson 
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.

Please enable JavaScript to use this website.