Emerson Launches Industry-first Controller Designed for Automation Versatility and IIoT-enabled Operations

DeltaV™ PK Controller simplifies capital projects, readies organizations for operational benefits of IIoT

AUSTIN, TEXAS (September 13, 2017) — Emerson is launching the DeltaV™ PK Controller, making the advanced automation of its DeltaV™ distributed control system (DCS) available to fast-growth industries traditionally less reliant on large-scale automation. The next-gen controller provides scalable automation control to all process industries, particularly parts of the life sciences, oil and gas, petrochemical, and discrete manufacturing industries that have relied on complex, non-integrated programmable logic controllers (PLCs) with limited operational capabilities. The fit-for-purpose DeltaV PK Controller is the process industry’s first controller that manufacturers can scale down for skid units or scale up to be natively merged into the DeltaV DCS in a larger plant.

Read More...
Click to continue reading

Today, these industries tend to use PLCs for smaller applications, which can create disconnected “Islands of Automation,” and limits plant production improvements. The DeltaV PK Controller is the first controller to truly bridge small and large control applications. Organizations can leverage the DeltaV PK Controller for effective, easy-to-implement standalone automation control akin to a PLC but with the features of a full-scale DCS, including advanced batch production, recipe management, execution, and historization. Users can then choose to leave the DeltaV PK Controller standalone, or natively merge it into their DeltaV DCS.  This capability eliminates operational complexity and dramatically improves the performance, safety, and efficiency of their entire project and operational lifecycle.

“The DeltaV PK Controller delivers a business-effective solution for organizations of all sizes to improve automation control and integration,” said Jessica Jordan, Emerson product manager. “The controller is capable of powerful standalone control for advanced automation on skids today while still being able to easily integrate into a full-scale DCS for total plant production control.”

The DeltaV PK Controller is the latest addition to Emerson’s Project Certainty initiative, targeting radical transformation in capital project execution. The new controller will simplify capital projects by enabling OEM skid-builders to design and produce skids in the same way they do today, while eliminating the costs, time, and risks associated with integrating a PLC into their control system.

The DeltaV PK Controller was designed from the start with connectivity, particularly into the IIoT, in mind.  The scalable controller leverages an assortment of communication protocols, including the first Emerson controller with a built-in OPC UA server. It is also the first Emerson controller with six Ethernet ports and can operate using any Emerson DeltaV I/O type, including DeltaV Electronic Marshalling, traditional marshalled I/O, wireless I/O, and integrated safety instrumented systems. In addition, it has built-in protocols to communicate with Ethernet devices such as drives and motors.  Together, these features make connectivity easier at every stage and help plants achieve operational benefits of cloud-based tools and analytics through the IIoT. The DeltaV PK Controller also features built-in redundancy for controllers, communication, and power supplies, allowing organizations to improve uptime without adding to complexity or footprint.

For more information visit, www.Emerson.com/DeltaVPKController

For more information on Emerson’s Project Certainty Initiative, visit www.Emerson.com/Project-Certainty

For a downloadable high resolution image of the DeltaV PK Controller click here.

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson on Wechat

About Emerson 
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.

Please enable JavaScript to use this website.